2008-04-17 9:07 PM
2011-05-17 12:52 AM
Hello. I have the following problem:
After a playing with a new code I lost the communication with STR911FA44X6 device via JTAG pins. In my last compilation I have change both clocks - PCLK and MCLK and maybe I made something wrong. I suppose that the problem is similar to this one: http://www.keil.com/support/docs/3215.htm But, I don't have a Keil JTAG probe. I'm using a Segger J-Link and IAR. Is there a way to make the same operation with J-Link? I have a Wriggler clone JTAG also.2011-05-17 12:52 AM
Hello mudrovc,
If you have an RLINK or Flash link, please try to make a full erase using CAPS? Best regards, mirou.2011-05-17 12:52 AM
Yes this helps. Thank you mirou. :)
I have a successful erase of the memory with FlashLink cable and JTAG Programmer software. Two things should be taken in account: 1. The FlashLink cable schematics has an error. A shortcut between DB8 & DB13 on PC connector is missing. Thanks to the guys from the forum http://www.st.com/mcu/forums-cat-4961-21.html I think the ST support team should correct the documents, the schematics didn't work without this connection.:( 2. To have a possibility to erase the locked chip you need to hold the device in RESET (via Assert Reset button). Hope this will help to other guys with a dead JTAG problem. :)We’re moving the ST Community to a new platform to give you a better and more reliable community experience.