2017-11-30 6:53 AM
I just uninstalled and newly installed the COSMIC stm8_32k compiler and applied for a new license, placed the newly received license in the License subfolder but I'm still getting the following error '#error cpstm8 C:\Program Files (x86)\COSMIC\CXSTM8_32K\Hstm8\modsl0.h:1 FlexLM No such feature exists.' I'm also not getting option to select the HKEY_CURRENT_USER or HKEY_LOCAL_MACHINE during installation. Anybody any idea?
2017-11-30 11:01 AM
Hello,
the stm8_32k compiler is old and is no more supported.
It has been replaced by the FSE version that has no limitations at all: you can doanload it
http://cosmicsoftware.com/download_stm8_free.php
Regards,
Luca
2017-12-05 7:20 AM
Thanks Luca,
that solved the problem.
Regards Egon.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.