2006-02-23 3:57 AM
Convert existing RS232-communication to USB
2005-08-28 11:18 PM
We have projects with RS232-communications from our hardware to PC. Now we create new hardware with STR710-processor and we would like to use USB insread of RS232. Is there an easy way, to modify the old software for this?
What have I to do, when I simply want to communicate from a PC to our hardware? Many thanks for good answers!2005-08-29 1:27 AM
Hi
I'm using uVision 3 from Keil with Keil-C-Compiler. Regards2005-08-29 9:50 PM
Hi,
I have ULINK and that is all ok. I'm speaking from the communication on target to PC. I have to write software for new hardware with STR710, that will communicate over integrated USB. I'm looking for software-examples to use USB. Regards2006-02-22 5:39 AM
I have the same task as yours.
Did you get something ?2006-02-22 11:57 AM
I have to write software for new hardware with STR710, that will communicate over integrated USB. I'm looking for software-examples to use USB.
Has anybody an example for Keil ARM ?2006-02-22 11:28 PM
Quote:
On 23-02-2006 at 08:55, Anonymous wrote: Hi, If you are using Keil uVision3, you can find an example for USB in the install directory of Keil (Keil\ARM\Examples\STR71xLibUSB) Rgds, Zouhair OK, i found an example for USB. Then i will make it as USB Bulk.2006-02-23 12:31 AM
I’m in search of a same example but for ST evaluation board MB393B.
If possible an example that use a standard driver… Thanks in advance, Stéph.2006-02-23 3:57 AM
I’m in search of a same example but for ST evaluation board MB393B.
If possible an example that use a standard driver… Thanks in advance, Stéph.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.