cancel
Showing results for 
Search instead for 
Did you mean: 

Controlling PSD I/O-pins on uPSD3354 uC

henk2
Associate II
Posted on May 15, 2014 at 11:18

Hi,

We need to modify one of our existing company products to be able to be controller by external I/O. The only externally available I/O-signals are the 6 JTAG pins. These JTAG pins are connected to the PLD I/O-Port C. I would like to control pins PC3 and PC4. But somehow I do not managed to get them active.

These next items are applied:

- set PC3 and PC4 to GP I/O mode in PSDsoft Express

- set the CSIOP to address 0x7F00 in PSDsoft Express (last 256 Bytes of the 32KiB SRAM)

- set the PC3/PC4 data direction registers (at address 0x7F14) to '1' (output)

- toggle PC3/PC4 output registers (at address 0x7F12)

But nothing happens on the outputs. Testing them as inputs also shows no results.

Maybe I forgot some setting in the PSD part of the uC?

thanks,

Henk
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.