2010-12-14 4:49 AM
has anybody ever used CCO, the configurable Clock Output? I think I initialized it. I enabled it. Everything compiled but I never did anything that would set the frequency. The output is a high. Does anyone know of an example or what I should be doing? I look thru the manuals and nothing seems to help me. It seems like such a simpe function but it is difficult for me.
charles2010-12-16 9:37 AM
» » » » »
examples/TIM1/TIM1_Input_Capture/main.c
00001
/**
00002******************************************************************************
00003* @file TIM1_Input_Capture\main.c
00004* @brief This file contains the main function for TIM1 Input Capture example.
00005* @author STMicroelectronics - MCD Application Team
00006* @version V1.1.1
00007* @date 06/05/2009
00008******************************************************************************
00009*
00010* THE PRESENT FIRMWARE WHICH IS FOR GUIDANCE ONLY AIMS AT PROVIDING CUSTOMERS
00011* WITH CODING INFORMATION REGARDING THEIR PRODUCTS IN ORDER FOR THEM TO SAVE
00012* TIME. AS A RESULT, STMICROELECTRONICS SHALL NOT BE HELD LIABLE FOR ANY
00013* DIRECT, INDIRECT OR CONSEQUENTIAL DAMAGES WITH RESPECT TO ANY CLAIMS ARISING
00014* FROM THE CONTENT OF SUCH FIRMWARE AND/OR THE USE MADE BY CUSTOMERS OF THE
00015* CODING INFORMATION CONTAINED HEREIN IN CONNECTION WITH THEIR PRODUCTS.
00016*
00017* <h2><center>© COPYRIGHT 2009 STMicroelectronics</center></h2>
00018* @image html logo.bmp
00019******************************************************************************
00020*/
00021 00022/* Includes ------------------------------------------------------------------*/
00023#include ''''
00024 00025/**
00026* @addtogroup TIM1_Input_Capture
00027* @{
00028*/
00029 00030/* Private typedef -----------------------------------------------------------*/
00031/* Private define ------------------------------------------------------------*/
00032/* Private macro -------------------------------------------------------------*/
00033/* Private variables ---------------------------------------------------------*/
= 2000000; = 0; =0, =0; 00037/* Private function prototypes -----------------------------------------------*/
00038/* Private functions ---------------------------------------------------------*/
00039/* Public functions ----------------------------------------------------------*/
00040 00041/**
00042* @brief Example firmware main entry point.
00043* @par Parameters:
00044* None
00045* @retval
00046* None
00047*/
void
(void
) 00049 { 00050 00051 ( , , , , 0x0); 00052 00053/* Enable TIM1 */
00054 (); 00055 00056/* Clear CC1 Flag*/
00057 (); 00058 00059/* Connect LSI to COO pin*/
00060 (, , ); 00061 (); 00062 (); 00063 00064 00065/* wait a capture on CC1 */
00066while
((->SR1 & ) != ); 00067/* Get CCR1 value*/
00068 = (); 00069 (); 00070 00071/* wait a capture on cc1 */
00072while
((->SR1 & ) != ); 00073/* Get CCR1 value*/
00074 = (); 00075 (); 00076 00077/* Compute LSI clock frequency */
00078 = (8 * ) / ( - ); 00079 00080/* Insert a break point here */
00081while
(1); 00082 } 00083 00084 00085#ifdef USE_FULL_ASSERT
00086 00087/**
00088* @brief Reports the name of the source file and the source line number
00089* where the assert_param error has occurred.
00090* @param file: pointer to the source file name
00091* @param line: assert_param error line source number
00092* @retval
00093* None
00094*/
00095void
assert_failed(* file, line) 00096 { 00097/* User can add his own implementation to report the file name and line number,
00098ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */
00099 00100/* Infinite loop */
00101while
(1) 00102 { 00103 } 00104 } 00105#endif
00106 00107/**
00108* @}
00109*/
00110 00111/******************* (C) COPYRIGHT 2009 STMicroelectronics *****END OF FILE****/
2010-12-16 9:41 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.