cancel
Showing results for 
Search instead for 
Did you mean: 

Case 1 5 GPS satellites with strong SNR & elevation angles above 10 degrees. Case 2 5 GPS satellites with a weak SNR & elevation angle above 10 degrees also. can case 2 be better than case 1 in positioning if the GDOP is better?

Mfathi50
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Once it has the navigation data, the SNR is less relevant.

It tends to be most important to see the direct signals, not multi-path/reflected ones.

The best solution is going to be the one with the least noisiest measurements.

DOP tends to be assumed to be a multiplier for the CEP specification.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.