2004-02-11 3:19 PM
Can you tell me why not generate the PWM warefore ?
2004-02-11 1:18 PM
The following is the relative code.It is used in the T72324,TIMERA Init_PWM
bset PFDDR,#4 bset PFOR,#4 ldb TAOC2HR,#$34 ldb TAOC2LR,#$E2 ;the period of pulse ldb TAOC1HR,#$3E ldb TAOC1LR,#$D0 ;the period of singal ldb TACR1,#%00000000 ;disable TimeA interrupt ,enable ICIE interrupt ldb TACR2,#%10010000 ;OC1E enable ,PWM mode bres TACSR,#22004-02-11 3:19 PM
I have solved it.
Quote:
On 2004-02-12 02:48, Rayon wrote: The following is the relative code.It is used in the T72324,TIMERA Init_PWM bset PFDDR,#4 bset PFOR,#4 ldb TAOC2HR,#$34 ldb TAOC2LR,#$E2 ;the period of pulse ldb TAOC1HR,#$3E ldb TAOC1LR,#$D0 ;the period of singal ldb TACR1,#%00000000 ;disable TimeA interrupt ,enable ICIE interrupt ldb TACR2,#%10010000 ;OC1E enable ,PWM mode bres TACSR,#2We’re moving the ST Community to a new platform to give you a better and more reliable community experience.