2007-04-06 10:06 PM
Can we work in debug mode using ICP algorithm
2011-05-17 12:40 AM
We are trying to boot from bank1.So we have selected ICP algorithms.With that we are able to download and execute.But we are not able to enter into debug mode.With icp algorithms is it not possible to debug or any other problem.Please help out.
Regards Anuradha2011-05-17 12:40 AM
Dear Ibtissem,
I am attaching the bmp file of the error.It is giving memory mismatch at location 0x00520002.But these are reserved values.There is no way of changing this.Is it necessary to use only ICP algorithms inorder to boot from bank1.Can you give more details about turbo programming mode.One more problem is once if we boot from bank1 we are not able to boot from bank0 again.Thank you for the reply. Thanks&Regards Anuradha.2011-05-17 12:40 AM
I got the answer.Problem is we should not use verify code download option in debug target options.Then it will work.We should not use verify option with ICP algorithm.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.