cancel
Showing results for 
Search instead for 
Did you mean: 

Can I connect the I2C, PC0 and PC1 pins , of the STM8L151K4, operating at 3.3V, to a bus with 5V pull-ups without any level adaptation?

JVica.1
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @JVica.1​, to the community!

Yes, PC0 and PC1 on STM8L151K4 are Five-vole tolerant (FT), which means you can communicate with a device that is powered by 5V, level translators are not required.

Good luck!

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @JVica.1​, to the community!

Yes, PC0 and PC1 on STM8L151K4 are Five-vole tolerant (FT), which means you can communicate with a device that is powered by 5V, level translators are not required.

Good luck!

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.