2006-11-02 6:20 PM
2006-11-02 1:33 AM
Hello,
I'm using BSPI0 and BSPI1: the BSPI1 is working well : we see MOSI / clck / MISO P0.4 : MISO P0.5 : MOSI P0.6 : CLCK P0.7 : not used in master = 1 P2.4 : CS equipment GPIO_Config(GPIO0,0x70,GPIO_AF_PP); BSPI_Init(BSPI1); BSPI_Enable(BSPI1); BSPI_MasterEnable(BSPI1,ENABLE); BSPI_ClkActiveHigh(BSPI1,DISABLE); BSPI_ClkFEdge(BSPI1,DISABLE); BSPI_8bLEn(BSPI1,ENABLE); GPIO_Config(GPIO0,1<GPIO_BitWrite(GPIO0,0x7,1); BSPI_TrFifoDepth(BSPI1,8); BSPI_RcFifoDepth(BSPI1,8); GPIO_BitWrite(GPIO2,0x4,0);//CS BSPI_BufferSend(BSPI1,buffer_send,8); while(BSPI_FlagStatus(BSPI1,BSPI_RFF))==0); GPIO_BitWrite(GPIO2,0x4,1);//CS BSPI_BufferReceive(BSPI1,buffer_receive,8); and with the same configuration for BSPI0 we don't have the clck but we have the MOSI? P0.0 : MISO P0.1 : MOSI P0.2 : CLCK P0.3 : not used in master = 1 P1.8 : CS equipment GPIO_Config(GPIO0,0x7,GPIO_AF_PP); BSPI_Init(BSPI0); BSPI_Enable(BSPI0); BSPI_MasterEnable(BSPI0,ENABLE); BSPI_ClkActiveHigh(BSPI0,DISABLE); BSPI_ClkFEdge(BSPI0,DISABLE); BSPI_8bLEn(BSPI0,ENABLE); GPIO_Config(GPIO0,1<GPIO_BitWrite(GPIO0,0x3,1); BSPI_TrFifoDepth(BSPI0,8); BSPI_RcFifoDepth(BSPI0,8); GPIO_BitWrite(GPIO1,0x8,0);//CS BSPI_BufferSend(BSPI0,buffer_send,8); while(BSPI_FlagStatus(BSPI0,BSPI_RFF))==0); GPIO_BitWrite(GPIO1,0x8,1);//CS BSPI_BufferReceive(BSPI0,buffer_receive,8); I see that the spi clck can also be a i2c : is it from this? Is the clck of BSPI0 is working on the str710? thanks2006-11-02 6:20 PM
I found why : I forgot for BSPI0 the configuration of PCU->BOOTCR
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.