2006-07-03 9:25 PM
2006-06-20 3:57 AM
Hello all,
We are currently using the BSPI0 on a STR71, with the fifos on. The depth is 7 words deep. The receive interrupt is configured to trigger when the receive fifo is full. However, it is set when we get only 1 word in it; it seems that both flags are set together (RFNE and RFF, respectively receive fifo not empty and receive fifo full). Is there something undocumented about those flags? Additionnally; where are those fifos mapped in memory? Are we only able to see the first word in the BPSI registers? Thanks for any input! Tech2006-07-03 9:25 PM
Hi,
I didn't have a time to check STR71x (I am working with STR73x) but as it is same family this should be same. FIFO is actualy on same address - all 16 of them. So for reading data from FIFO you can do something like this: for(i=0; iRXR); } You are practticaly reading same addres 7 times but every time receiving new byte. It is same procedure for writing in - you write byte after byte on same address. I hope this will help.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.