2005-09-02 5:58 AM
2005-08-24 4:14 PM
Hi guys,
I would like some advise if its possible to declare a variable of 24 bits and manipulate each single bit like setting bits? Rgrds, ongth602005-09-01 5:30 PM
Hi,
This is using the GPIO as an example, mayb i dun understand how do i use it as a general variable where the size is of the variable is 8 bit and i can manipulate each single bit and when i were to store, i can store the whole byte all together, like creating my own settings: struct{ u8 Regular_Reporting_Time : 3; u8 Non_Violation_SMS_Enable : 1; u8 Vibration_Enable : 1; u8 Smart_Powersave_Enable : 1; u8 FLEET_Type_Enable : 1; u8 Voice_Call_Enable : 1; }Byte3_Setting; Regular_Reporting_Time = 0x04; Vibration_Enable = 0x01; EEPROM_byte_write(Byte3_Setting); Rgrds, ongth602005-09-02 5:58 AM
ongth60,
You first have to allocate a variable for a Byte3_Setting structure. Then you can access the bit fields through normal structure member access (i.e. dot notation)...for example void SaveSettings(void) { struct Byte3_Setting mySettings; mySettings.Regular_Reporting_Time = 0x04; mySettings.Vibration_Enable = 0x01; EEPROM_byte_write(Byte3_Setting); } This example isn't particularly practical, but that's how you can use your structure. In a more practical usage you would probably want to allocate your variable somewhere else and pass a pointer along with settings to fill in but remember then you would access the members using the -> operator like: void SaveSettings(struct Byte3_Setting *pSettings, int reportingTimeValue, int vibrationEnabled) { pSettings->Regular_Reporting_Time = reportingTimeValue; pSettings->Vibration_Enable = vibrationEnabled; EEPROM_byte_write(*pSettings); } Also check your compiler documentation to make sure you understand how it handles bit-fields and structure packing as this can sometimes be a problematic area. Hope this helps. Ryan.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.