Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TIM3 wrong counting?

Posted on September 04, 2012 at 17:14I need to generate a 20 ms interrupt into my firmware. HSE is 16 Mhz with STM8S208. I put this initialization code into my firmware to accomplish that through the use of TIM3: #define PRESC TIM3_PRESCALER_32     ...

STVD 4.3.1 : swim error [30103]

Posted on February 09, 2012 at 12:26Hi, I'm running windows 7 64 bit, my target is STM8S103F2U. STVD gives me this error when trying to debug: ''failed to download application: error: swim error [30103]: rlink communication error''.    Rlink does no...

@eeprom

Posted on August 09, 2011 at 18:31Anyone know how to use the @eeprom on the cosmic compiler Does it suppot @eeprom vu32 EE_Total; The above passed the complier but if I try to use it I get errors I've also tried char and int but none seem to work. ...

Breadboard friendly to the STM8L-Discovery?

Posted on August 20, 2012 at 10:30I've got an STM8L-Discovery and am having loads of fun with it.  I would like to go beyond flashing two LEDs and writing stuff to the LCD display, however, which means I'd like to breadboard.  The problem is that th...

STM8S003F3 chip and GPIO

Posted on August 15, 2012 at 04:33Hi all! I'm working with STM8S003F3 chip on my project and I'm have some problem about it, i wana help of ST technician. on my project,i using pin4 and pin5 of port B to control normal IO applications,I have alrea...

ST Visual Develop Multiple Instance Issue

Posted on July 26, 2012 at 09:57Hi Guys,I'd like to work on multiple projects at the same time using STVD. But it does not permit to open a second instance. I dug in to the options and help, but couldn't find any clue about this subject. Is there a ...

Can't configure Timer2 configuration registers

Posted on August 13, 2012 at 16:15Hi. I'm trying to use Input Capture mode on Timer2 (channel 3) on an STM8S105 (discovery board). It won't work, and when i m watching peripheral registers with appropriated breakpoints, the registers aren't changing...

thibaut2 by Associate II
  • 957 Views
  • 2 replies
  • 0 kudos

STM8S interrupts

Posted on August 08, 2012 at 17:37Can someone direct me, a newbe to hardwire interrupts, to a pdf file telling me how to use an interrupt on the stm8s207? I want to run the stm8s continuously and retrieve information by command from and master contr...

carnett1 by Associate II
  • 1142 Views
  • 1 replies
  • 0 kudos

STM8 code size

Posted on July 25, 2012 at 11:59Hi, I am new here, and new with STM8. I wrote some code and it works fine :). For final production I want use smaller STM8. Where can I find how big is code? I want use a STM with flash memory as small as posible (or ...

sm2 by Associate II
  • 1125 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.