Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

M24LR discovery Linker error

Posted on March 11, 2014 at 18:09Hello, I am having an error message when I build my codes using the ''release'' mode in order to generate the .s19 file before programming my MCU. Running Linkerclnk -lC:\Lib  -o Release\discover.sm8 Release\discover...

roddyrpg by Associate
  • 1243 Views
  • 1 replies
  • 0 kudos

DAC parasitic pull-up?

Posted on June 03, 2014 at 20:52I have working code for DAC testing, and it works fine on STM8L152C6 (Discovery board), but meet some problems with STM8L152K6. It works about as expected, excepting output has permanent additional value 0.88V. I trie...

igor by Associate II
  • 1741 Views
  • 1 replies
  • 0 kudos

Cosmic Linker - absolute memory address problem

Posted on May 29, 2014 at 12:17Hello, I'm using Cosmic STM8 32K Special Edition Free license v. 4.3.11 under STVD IDE. MCU: STM8L151 I'm trying to place 4 bytes with specific values into absolute memory address. I found in manual and even on cosmic ...

bogusz by Associate II
  • 1605 Views
  • 2 replies
  • 0 kudos

STVP use for more than serial number string

Posted on May 28, 2014 at 00:36We use STVP (v3.3.1) for programming parts.  I'm in the process of adding the Serial Number, using that feature in STVP.  But we have a number of stations, and so each has unique identifying information.  For example,...

mike23 by Associate II
  • 1929 Views
  • 3 replies
  • 0 kudos

Stm8s touch sensing

Posted on May 28, 2014 at 12:58Hello am making control panel using stm8s105 controller and springs electrodes. Everything works fine but some times device become extra sensitive and  all touch buttons making switch on in a random way without any con...

Pull Up pin

Posted on May 26, 2014 at 20:55Is there some way to turn off a pull up input for some time and later turn it on on a certain frequency? The pull up pin drain too much current.

bruno2 by Associate
  • 1738 Views
  • 3 replies
  • 0 kudos

STM8S interrupt latency

Posted on February 12, 2013 at 01:29What is the interrupt latency on STM8S MCUs? I am new to STM8 and the few docs I have read do not mention it.

rg1540 by Associate
  • 2596 Views
  • 4 replies
  • 0 kudos

STR912 Partiry bit set Error.

Posted on April 09, 2014 at 13:48hi.dear i use to IAR compiler, default_form_lib_2.1_iar_5.30 library and jlink. it is my developer environment.  my chip is STR912FAW44. first. i initialize UART2 set None parity bit. second. i change to UART2 set  ...

ikassma by Senior
  • 1490 Views
  • 3 replies
  • 0 kudos

Register Bit Definitions

Posted on May 22, 2014 at 13:09Dear All,I've been discovering STM8 core capabilties and properties for a while. I've had a chance to read datasheet for STM8L152. But I couldn't find detailed register info. For instance, CCR (Condition Code) register...

batu by Associate
  • 868 Views
  • 2 replies
  • 0 kudos

Generate beep on STMT/8L-EV1

Posted on May 15, 2014 at 20:15I have the STMT/8L-EV1 and I'd like to generate a 4KHz beep sound when one of the directional buttons is pressed.  Seems straight forward but I'm not sure how to implement it.  I've tried just using and turning the GPI...

connor by Associate II
  • 2511 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.