Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

where to buy stm8 in india?

Posted on September 09, 2015 at 14:35hello, what are the places where we can buy STM8 micro controllers in india? i dont see them available in retail shops. one place where i can get is from element14 through online, but it is costly. please share i...

kumaresh by Associate II
  • 2190 Views
  • 3 replies
  • 0 kudos

[ATT]10705

Posted on January 05, 2018 at 20:00Measuring three phase using ADC Hello everyone, I have a problem with measuring ADC.I am building a  device with the ESP8266 + STM8S003F3P6 module which will have 3x230V network voltage measurement and transmission...

[ATT]10688

Posted on January 03, 2018 at 23:20stm8s103f2 is not able to program hex my product's board is based on stm8s003f3 mcu(TSSOP 20pin), but there was some problem in providing the chipset,so I bought stm8s103f2 TSSOP20pin instead of buying stm8s003f3.T...

Simon Lee by Associate II
  • 3216 Views
  • 4 replies
  • 0 kudos

STM8 how to change Duty Cycle during running

Posted on January 04, 2018 at 13:40Hello community,i try to programm an code for my experimentation and i have a problem .. my code should change the duty cycle ie. the value of CCR2_V if the value of Convertion_Value_Current exceeds or is below a s...

STM8S001J3 open-drain mode

Posted on December 15, 2017 at 08:22HiI would like to use open-drain mode for PB5 pin of STM8S001J3.GPIO_DeInit(GPIOA);GPIO_Init(GPIOB, GPIO_PIN_5, GPIO_MODE_OUT_OD_LOW_FAST);I do not know why the voltage goes down even if I set it like the code abo...

FORTH for STM8S-Discovery

Posted on July 20, 2010 at 07:08Here is a FORTH interpreter-compiler for Discovery Board.  It is in the form of an assembly file stm8ef.asm.  You can assemble it on STVD and download it to Discovery.  You need a UART connection to Hyperterminal on P...

ting by Associate II
  • 5503 Views
  • 14 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.