Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

community.st.com

Posted on December 20, 2017 at 12:33STM8 2018 wishlist There is a https://community.st.com/community/stm32-community/stm32-forum/blog/2017/12/05/2018-stm32-wish-list but none for the STM8 yet, so I'm starting one here.Philipp#wishlist

Problem with External intetrupt flag clearing

Posted on March 19, 2018 at 00:25Hello guys.I've recently downloaded ST standard libraries for stm8s series and working with the functions.In cube mx version when we called an interrupt the callback function automatically was executed and after that...

read and write memory from M95080-w

Posted on March 22, 2018 at 14:30Hello everyone,I am trying to read and write memory from M95080-w eeprom using um232H-B spi communication.Whenever I read from eeprom i am getting 0xFF as out. If anyone had similar problem please share your ideas or...

GPIO control on BlueNRG2 Sleep

Posted on March 20, 2018 at 13:23Hello,I am using BlueBRG 2 on a low power application. My device is communicating using SPI to an external device. When I try to go in low power mode, the lowest current consumption that I can achieve is around 90uA....

stm8 cosmic problem on stvd

Posted on June 14, 2016 at 11:12Hi friendsI'm new with stm8 microcontrollers, i have download st peripheral library and stm8 cosmic free compiler. after building project i see this errors:--------------------------- Project 5 - STM8 Cosmic - Configu...

Which libraries should I add to the project?

Posted on March 16, 2018 at 20:36Hello.I'm trying to get started with stm8s series with IAR compiler that I'm not very good at.So for the first project just trying to on and off a single LED to see if everything is ok or not.I used Keil before this ...

I used the eDesign Suite set up a Flyback converter for the L6566. I need help with the compensation

Posted on March 15, 2018 at 22:08I used the eDesign Suite set up a Flyback converter for the L6566.   The compensation loop design looked unreasonable with 'Ropto' being only 51Ohms (output is 26V).  It would need to be 9W while attempting to source...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.