Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cannot get timer1 channel 3 or 4 to PWM

I cannot get timer 1 channels 3 or 4 to output a PWM. Here is how I have it initializedstatic void _vBl_initGauge_PWM(void) { TIM1->PSCRH = (u8)((sBL_PWMoutConst.PSCR >> 8) & 0xFF); TIM1->PSCRL = (u8)sBL_PWMoutConst.PSCR; TIM1->ARRH = (u8...

Using SWIM and STM8S to send hex file to 24c64wp

Hi all. I am a complete newbie with regard to the world of the STM8 and the programming of it so there are very high odds that I will completely use the wrong terminology in order to express what I think I know and also what I am working to acheive.....

MFarl by Associate II
  • 4822 Views
  • 6 replies
  • 0 kudos

Help with power supply of STM8L152C6T6 MCU

Hello,I'm designing a PCB using the STM8L152C6T6 communicating with an M24LR04E-RMC6T via the I2C protocol. Currently, I'm struggling to understand the power supply schema. According to the datasheet, VDD1, VDD2, and VDDA pins must be connected to an...

L9733 Hardware integration and SPI access

Hi,I designed a board integrating a High Side L9733.I try to communicate with the switch through SPI but I miss some informations.1- Can you confirm that we can use a 1.8V SoC as master?I fixed VDO to 1.8V. I didn't find nominal range for VDO. (only ...

rmt37 by Associate
  • 1100 Views
  • 0 replies
  • 0 kudos

Is VNQ7140AJTR discontinued?

I'm trying to get a hold of 500 units of VNQ7140AJTR and I've been unable to find any in stock at any distributor. I placed an order with Digikey about a month ago and it has been on back order since then. They are not able to give me an expected del...

KGreg by Associate
  • 757 Views
  • 0 replies
  • 0 kudos

hello sir, problem with debug - st-link

i installed the latest stvd, in windows 10.i try a program, for the discovery board., its ok with compling, and build, but when i want to debug, it say " connection error (usb:/usb):gdi-error (40201)can't access configuration databasei can read out t...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.