Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Example code for STM8S003F3

I am working with STM8S003F3 in our custom board . I need to communicate with an transceiver through SPI. I need a sample code for configuration of SPI in master mode and write /read process in SPI. Pls support by providing sample project.

spark.1 by Associate
  • 1189 Views
  • 0 replies
  • 0 kudos

Hi, L6387ED is used in STM's B-G431B-ESC1 which uses 3.3V logic when the L6387ED is only rated for 3.6V minimum high level logic threshold. Can L6387ED be reliably used at 3.3V? Please see additional details below.

The L6387ED datasheet indicates that the high level logic threshold is 3.6V as a minimum. https://www.st.com/resource/en/datasheet/l6387e.pdf#page=7The STM ESC eval kit (P/N: B-G431B-ESC1) definitely uses the L6387ED. We checked schematics and a some...

DRech.1 by Associate
  • 1079 Views
  • 0 replies
  • 0 kudos

USART Communication with PC (stm8al3l68)

Hello,I'm trying to implement serial communication between a stm8al3l68 an a serial terminal installed on my PC.The problem is that there is no virtual port on my STM8 as on STM32.How can I communicate with the PC if there is no virtual Port. What ki...

AJT by Associate III
  • 1841 Views
  • 3 replies
  • 0 kudos

Power Draw with ADC on STM8L152C6

I'm attempting to program this chip to act as a thermometer that can run on a low power solar panel. The issue I'm having is the power draw is way too high. Halted i have the power draw with an LCD and RTC interrupt ready at 5.5uA, but when I'm using...

SJack.1 by Associate
  • 756 Views
  • 0 replies
  • 0 kudos

About TIM1 in STM8L series. I have been trying default PWM testcase available by STM for modulating Duty channel and frequency. I change values of TIM_PERIOD and CCRx_Val. I only see frequency changing. For some reason I observe only 50% duty cycle.

For some reason I am not able to see pins behavior in plotter. I am not able to see PD 2,4,5 output on plotter on STVD tool.I got the testcase from https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm8-embedde...

RShah.3 by Associate
  • 740 Views
  • 0 replies
  • 0 kudos

Stvd newbie

I've generated an output file from STVD in .elf format. But stvp requires motorola hex format. Do I have to do another conversion?

Elong.1 by Associate II
  • 1369 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.