Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

M95M01-A125 in half duplex mode

Can the M95M01 work in half duplex mode? The Master has a 3 wire SPI interface with one open drain DIO. From the timings it looks like the M95M01 output is in high impedance whenever the master is accessing the bus. When the slave is answering the ma...

gcele by Associate
  • 739 Views
  • 1 replies
  • 0 kudos

Resolved! ST VD Software installation Issue : An anomaly (1) has been detected during installation.

Hi Team,I have installed ST Visual Develop in ST web page. At the end of installation, installation page got stuck and then i have terminated by end task using task bar....After completion of installation, i have opened software then following error ...

STNRG328 Bootloading procedure

Hi All,​There are a questions about AN4656 Application note,while I am trying Access EEPROM by following this document.Where is the file(*.s19) mention in Chapter 8 .I have been searching on the ST official website, but found nothing.How do I obtain ...

CHsia.2 by Associate
  • 956 Views
  • 0 replies
  • 0 kudos

Resolved! Applying voltage to the output pin of STMPS2171STR

Hi,Currently, I have two boards that contain a 5 volt power supply. Due to flexibility for future projects, both of are powering the same pin on a connector. The STMPS2171STR was added to one of the boards to cut the voltage going to the connector. H...

MOliv.1 by Associate II
  • 1963 Views
  • 7 replies
  • 0 kudos

Truth Table for STHV800L?

Hi,the included data brief in ST site does not provide the function of input pins. Like a truth table as to how to control different channels I was wondering if someone can provide me with the same..Thanks in Advance.Thanks and Regards,Siva

SSR by Associate
  • 753 Views
  • 1 replies
  • 0 kudos

STM8 Eclipse device descriptions (XLM/SVD)?

hello all,I am currently trying to add STM8 peripherals to the Eclipse embsysregview plugin. For this I would need device descriptions in XML or SVD. For STM32 ARM devices these are published as SVD files (see e.g. https://www.st.com/content/st_com/e...

GIcki by Associate II
  • 5233 Views
  • 4 replies
  • 1 kudos

Resolved! EEPROM WriteProtection

hey allI am using EEPROM library in the link belowhttps://github.com/sinadarvi/SD_HAL_AT24/blob/master/at24_hal_i2c.cI used the code successfully and it worked properly. I am using AT24C32. there is a WriteProtection pin on it, without enabling it, ...

Ala by Senior
  • 1298 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.