STEVAL-IPFC01P1 Load Current Limitation
we are using STEVAL-IPFC01P1 load current is limited to 4A. If it is exceeded we Fault occurs and LED turns RED. Provide support in this regard
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
we are using STEVAL-IPFC01P1 load current is limited to 4A. If it is exceeded we Fault occurs and LED turns RED. Provide support in this regard
Hello!Datasheet does not show VFBN connect to Vin and shows ADIM need to connect to LDO3 or resistor to gnd. However, eDesignSuite schematic shows that. I want to know why . Could you help me to figure out these design? Thank you~
INTERRUPT_HANDLER(EXTI_PORTA_IRQHandler, 3){ /* In order to detect unexpected events during development, it is recommended to set a breakpoint on the following instruction. */ if(!GPIO_ReadInputPin(RUIDO_PASS_Port, RUIDO_PASS_Pin)) { Tmr10msLeRuid...
We are using STEVAL-IPFC01V1, Evaluation board. We tried to replace Inductor with our customised inductor and toroidal core. Inductance value is 125uH. We are detecting a fault for loading to 7A. Board works for 4A but for 7A fault is detected, outp...
I have a STM8S003F3 and a Arduino Micro SD Card Module. I want to communicate with Micro SD Card. But Project SPI_FastCommunicationMicroSD in STM8S_StdPeriph_Lib is not working. It goes into "Go to infinite loop when there is mismatch in data program...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.