Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

x-nucleo-idw01m1 firmware

Hello,I have a x-nucleo-idw01m1 and i'm trying to update it's firmware... Reading online i figured out that the latest version is 3.6 but i cannot happen to find the binary image anywhere, all of the links provided are broken.Does somebody still have...

NQui.1 by Associate
  • 853 Views
  • 0 replies
  • 0 kudos

Hi all, My question is about the stm8 series. I am currently working with stm8s001jm3 and am trying to generate 2 MHz from a pin. The problem is that I can only generate a maximum of 380 kHz, although I have set everything correctly.

Im using the COSMIC Toolchain with the standard library.Here is the setting:##########################################################void clock_init(void){ CLK_DeInit();              CLK_HSECmd(DISABLE); CLK_LSICmd(DISABLE); CLK_HSICmd(ENABLE); whi...

ATürk.11 by Associate II
  • 3340 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.