Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8L050J3 wfe() wakeup using TIM2 timer.

Good morning. I've been trying for a while to put the MCU in low power with the wfe() instruction and wake it up with TIME2 but the MCU gets stuck in wfe() and doesn't wake up. With the debugger active it seems to work even if it doesn't respect the ...

GBran.2 by Associate II
  • 4271 Views
  • 4 replies
  • 0 kudos

M24C16-RMN6P Address pins

Hello everyone, It is not clear on M24C16 datasheet, the meaning of A10, A9, A8 (see figure) about chip enable address. My question is, which is the I2C address for this device?Is it possible to use two of this devices on the same I2C bus?T...

0693W00000bhNuXQAU.png

Using Interrupts with Cosmic on STM8AF5288

Just changing over to the STM8 using STVD and Cosmic.I have converted an existing project over to the new chip and compiler and have a clean compile of all the modules. The Linker is complaining that #error clnk Debug\5971.lkf:1 @svlreg missing for ...

BCowa by Associate II
  • 2199 Views
  • 1 replies
  • 0 kudos

STM8S003 vs ES7P003

Hello,​W1209 W1219 W3230 boards and several others of Chinese origin are usually equipped with STM8S003. But I got a board with ES7P003FGTF.​It looks like a PIC inside the body of an STM8. Programming system uses Data and Clock, and no capacitor pi...

0693W00000bhQrZQAU.jpg 0693W00000bhQrPQAU.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.