Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

lcd interface

Hi all, I am currently working to interface a 16x2 LCD(LM016L) display with STM32F103C8 through MCP4725. The problem I am facing is that while comparing a similar work I could not find the relevant libraries. I am also new to STM32IDE so I might not ...

Mosfet marking e3 G

Hello,I am wondering at point did ST drop the G from the marking?These parts are made in 2023, the older models had ST  e3 G on the first line. 

besagm_0-1695645122524.png
besagm by Associate
  • 1977 Views
  • 1 replies
  • 0 kudos

ER GP 350 No Datasheet

Hello to all !I have a pumping system where it has this SMD component inside and I can't find the datasheet to check its status.Can anyone help me?Thank you very much

scosta by Associate
  • 1706 Views
  • 1 replies
  • 0 kudos

STNRG012 and STEVAL-PCC020V2

Hi, I hope you can help me. I'm working with STNRG012 on a power supply. we have already done the prototype, how ever we can make it run due to that STNRG012 needs a programming device (STEVAL-PCC020V2). This device is active but out of stock and I c...

Resolved! LD1117S33CTR design problem

In our company's mass production product( we desgien and produce BLDC motor driver). We stumble across  that in some PCBA (about 25% of all the mass production)  the LD1117S33CTR output have voltage oscillation.Becasue of the 3.3V output is for MCU c...

2021903727.jpg 电路图.JPG C73更换1uf电容.jpg
XiZhao by Associate II
  • 3389 Views
  • 5 replies
  • 2 kudos

LSM9DS1 interrupt pulse

I have configured Gyro and Accelerometer to generate interrupt on Data-Ready event on Int1 and Int2 pins. I also left at default 0 value bit LIR_XL1, which, according to the documentation, makes interrupt request NOT latched. However, when I power-on...

AZ1101 by Associate
  • 830 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.