Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! 74LCX541/SO

Hello Everyone,I am facing problem in ADC section of  our project schematic. We are using ADS8505 Analog to digital converter as the output of ADC ranges from 0v to 5V and microcontroller which we are using(STM32F413ZGT6) is connected to 3.3 Volts su...

Rushali by Associate III
  • 4101 Views
  • 4 replies
  • 1 kudos

Resolved! STGAP2SMTR pin configuration regd

We have recently bought the STGAP2SMTR from DIGIKEY. The pictures of the same is attached to this. I am unable to figure out which pin is pin number 1 (there is no DOT in the IC). Please can you look at the pictures and let me know which is the pin n...

Resolved! Finding a suitable Mosfet

I am working on reparing a battery charger for a campervan and searching for a replacement for Mosfet partnumber h7na80fi.Is there any suitable one?

JErik.1 by Associate II
  • 3505 Views
  • 4 replies
  • 1 kudos

Reading mapfiles - a tool for you

I have seen a number of questions about reading the stm8s mapfiles and I was also someone who struggled so the attached tool might be helpful (and do let me know of any errors!).The key elements are:- There are some elements that are stored in ROM ("...

Resolved! STUSB4500 I_SNK_PDO_FLEX

I can’t find a description of this (I_SNK_PDO_FLEX) parameter, what it is for, and what it affects in the decision-making algorithm about the power profile.Thanks.

Stas_0-1710441090608.png
Stas by Associate
  • 1566 Views
  • 1 replies
  • 1 kudos

STVisual Develop building libraries

I have a very simple main using UART1 and already my application is 7kB!  The web implies that this is because I am getting a lot of UART1 and CLK code built and linked in that I am never using.  One suggestion is to split the UART1 and CLK files int...

Ensure code running in RAM

Ref: stm8s flash entire new program - how? - STMicroelectronics CommunityHow do I ensure that an entire routine, and anything that it might call, is running in RAM?  I think there is a RAM() macro around, for example, the flash write methods so can I...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.