2007-01-14 9:11 PM
2011-05-17 12:35 AM
Do I need to add an external latch in order to interface the processor to a 1Mx16 SRAM chip?. I know is a basic question, but it seems that the documentation I'm reading suggests that an external latch is not needed: based on ''Insider's guide'' by Hitex (p.54) or on the reference manual (p.37. ''Mux mode with 16-bit data, 24-bit address'')
2011-05-17 12:35 AM
Depends on the device you are connecting to.
Most Flash/SRAMS will require the external latches as they do not support multiplexed addressing. The datasheet of the part you are using will tell you what mode it supports. Regards sjoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.