2018-08-03 2:39 AM
I'm trying to compile an example from "ST Aseembler Linker", Chapter 4.4 "Segmentation"
stm8/
segment byte at: 0 'code'
segment byte at: 8000 'ram'
segment 'ram>code'
label1: nop
endand i get the following error:
Error in map file Debug\00_test.map: wrong map file format: can't find segment type!
The command: "abslist Debug\main.lsr -exe Debug\00_test.s19" has failed, the returned value is: 1
exit code=1.
file 00_test.map has next contains:
Segment List
------------
c:\users\flanker\documents\stvd\00_test\main.asm[3] 4- 7 0 - 0 'code'
c:\users\flanker\documents\stvd\00_test\main.asm[4] 4- 7 8000 - 8000 'ram' [text]
Class List
----------
0 ' code' byte from 0 to 0 (lim FFFFFFFF) = 0% D
0 ' ram' byte from 8000 to 8000 (lim FFFFFFFF) = 0% C
External Label list
-------------------
Symbol Name Value Scope Def(line)
0 labelsWhat am I doing wrong?
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.