2009-05-24 10:59 PM
Are there any difference between SPI0 and SPI1???
2011-05-17 12:58 AM
I need to use SPI1 an a motorola style master, but I can't recive. If I use the same code on SPI0 it works fine.
I can set SPI1 in loopback mode. I have verifeid the electrical stuff. I use P3.6 and P3.7. Is there anyone that have experience of SPI1 at P3?? Regards OlaWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.