2009-05-05 9:42 PM
2009-05-04 3:29 AM
Hi,
I use ST7lite29 with internal oscillator. My options bytes are: Write Protection: OFF Read Out: ON SEC: 4K OSCRANGE: ReservedWDG_HALT: not reset in halt WDG_SW: Software LVD: medium OSC: RC oscillator ON PLL Enalbled and X8 Programmer: Indart STX With this setting the watchdog don't work. :-[ If I setting: OSCRANGE: MP:2-4MHz work!!! :D Question: is it correctly setting ''MP:2-4MHz'' when I use internal OSC? What's I must select? Thanks2009-05-05 9:42 PM
Hi Cicciounico,
in my opinion ''reserved'' means reserved for further application and should not be used. Have a look at chapter 15 DEVICE CONFIGURATION: Note: When the internal RC oscillator is selected,the OSCRANGE option bits must be kept at their
default value ...The default value for OSCRANGE is 111 = External Clock Source: CLKIN at PB4. In my application it works fine with this setting. Regards, WoRo
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.