2008-02-05 2:43 AM
2011-05-17 12:49 AM
Hi folks,
I just don't get it: I configured the ADC according to the reference sheet. The ADC does start the conversion and produces an ECVI. But there are no data (voltage was about 2,2V). Here is my code (relevant parts): /*********** CODE ***********/ init_peripherals.c: (...) void init_ADC(void){ // Clock for ADC SCU->PRR1 |= 0x00040800; SCU->PCGR1 |= 0x00040800; // Configure channels ADC->CCR = 0x000C; // RESET // Set GPIOANA for 4.1 SCU->GPIOANA = 0x0002; // configure options ADC->CR |= 0x0440; // ECVI enable, single channel mode on ch1, one shot mode // Set POR ADC->CR |= 0x0002; // wait 1ms wait(1000); // STANDBY // clear STB ADC->CR &= 0xFFF7; // wait 15 us wait(15); // IDLE // conversion needs to be started by setting STR } void init_VIC(void){ /* VICx_INTSR, set corresponding bit [0: IRQ; 1: FIQ] * VICx_VCiR, enable corresponding register with 0x20 and pass IRQ# to 0:4 * VICx_VAiR, pass address of ISR * VICx_INTER, set corresponding bit [0: dis; 1: ena] */ // Clock for VIC SCU->PRR0 |= 0x0020; SCU->PCGRO |= 0x0020; // Interrupt for ADC VIC0->VCiR[15] = 0x20; VIC0->VCiR[15] |= 15; VIC0->VAiR[15] = (unsigned int)ADC_IRQHandler; VIC0->INTER |= 0x8000; } main.c: (...) // measure U_LDR_offen ADC->CR |= 0x0001; wait(500); (...) /*********** END OF CODE ***********/ Do I need to set GPIO4.1 to Alternate Input (internal peripheral connected)? This is what they do in the Blinky-example. Haven't tried this yet. HARDWARE: Keil MCBSTR-9 (STR912FW44) Keil uvision Cheers Nik2011-05-17 12:49 AM
Hello Liqnik,
''Do I need to set GPIO4.1 to Alternate Input (internal peripheral connected)?'' No you should configure the GPIO in analog input mode. However, you can only configure it in analog mode (in SCU_GPIOANA register) since the GPIO has the input as the default mode. Could you please refer to the v2.0 library to the first example of the ADC (the end of conversion interrupt is used). Best regards, mirouWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.