2010-12-24 1:20 PM
Hi all,
Here's an improved code for the 4x3 keypad with debounce and autorepeat. With STM8S 2MHz clock it performs pretty close to the PC keyboard. The action() function is out from the keypad management state machine for clarity. Suggestions and improvements are welcome. Hope it helps. Merry Xmas and happy holidays Steven u8 key = 255; u8 oldkey = 255; u8 AutoRptMax = 64; u8 AutoRptCount = 0; while(1) { key = GetKeyPressed(); //Scan the keypad to getting the code of the key pressed // < Is it a valid key pressed ? > if (key < 12) // YES { // < Is key still the old one ? > if (key == oldkey) // YES { // (Start counting for autorepeat to occour) DelayMS(50); AutoRptCount++; // < Is time to execute the key action? > if (AutoRptCount >= AutoRptMax) // YES { Action(key); // perform the action according to the key code AutoRptCount = 0; // reset the autorepeat counter to get ready for the next autorepeat event AutoRptMax = 16; // make the autorepeat limit short for speeding up the next repetition when keeps keypressing } } else // NO, the key is new brand { Action(key); // perform the action according to the key code DelayMS(50); // and also make a little debouncing } } // END if (key < 12) else // NO, the key is not among the 12 defined keys { // < Was the key pad released ? > if (oldkey < 255 ) // YES { AutoRptCount = 0; // reset the autorepeat counter AutoRptMax = 128; // and restart using the first typing delay long } } oldkey = key; } void Action(u8 key) { switch(key) { case 9: // backspace (mode entry is ''right after writing'' so we need to cursor left twice) LCD_DATA(0x10,0); LCD_CHR(32); LCD_DATA(0x10,0); break; case 11: LCD_DATA(0x14,0); // cursor right break; default: LCD_CHR(key + 48 + 1); // display keycode break; } } void DelayMS(int delay) { int nCount = 0; while (delay != 0) { nCount = 100; while (nCount != 0) { nCount--; } delay--; } } #stm8s #debounce #autorepeat #4x3-keypad2010-01-02 11:21 AM
ok,
the original thread was updated. Please remove this one if you would. Thanks SP2010-12-27 5:50 AM
''Here's an improved code for the 4x3 keypad''
I guess your ''improvement'' relates to this: [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM8SDiscovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM8SDiscovery/Discovery with LCD and 4x3 keypad example&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000CCDF802E596CAF44ADED5E61F5CA8B1B]https://my.st.com/public/STe2ecommunities/mcu/Lists/STM8SDiscovery/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fSTM8SDiscovery%2fDiscovery%20with%20LCD%20and%204x3%20keypad%20example&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000CCDF802E596CAF44ADED5E61F5CA8B1B You should also update that thread with a link to this ''improvement''...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.