2025-02-24 12:25 AM
We need 24 bit low speed adc, i have found HX710B is low cost and 24 bit----but one big problem is it is chines manufaturer.can we use it for weighing scale with stm32f103 or stm8 series MCU reliably
2025-02-24 1:04 AM
>... -but one big problem is it is chines manufaturer.
I don't know why this is a problem.
If you can source the IC itself and find the datasheet, you are fine.
It probably has a SPI or I2C interface, and there are plenty of driver examples.
> We need 24 bit low speed adc, ...
I suppose you know what you are doing.
Designing a proper hardware for a 24-bit ADC and really achieve nearly the accuracy and stability the 24 bit promise is far from easy.
2025-02-24 2:05 AM
@BAS-BLEU wrote:one big problem is it is chines manufaturer.
As @Ozone said, why should that be a problem? A microcontroller cannot tell the nationality of external components!
@BAS-BLEU wrote:can we use it for weighing scale with stm32f103 or stm8 series MCU reliably
As for any other component, you just need to study its datasheet, and see if what is specified there is compatible with the capabilities of your chosen microcontroller:
http://www.8052mcu.com/forum/read/160143
As @Ozone suggested, achieving anything like 24-bit accuracy in practice requires very careful, precision analogue design!
2025-03-10 6:20 AM
actually chines chip generally not dependent for R&D. i have faced lot of issue like LM324,UC3842,UC3843 that were also chines and i have designed SMPS but it redululosly failed . the chip as per data sheet pin mapping is different than procured chip. thats the 30 days of wastage of time of using chines chip.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.