2006-05-28 1:16 PM
2011-05-17 3:09 AM
Hi All,
I am working with uPSD3400 and I intend to work with the two UARTs. Is it possible to use one timer (TIMER2) for both of the UARTs? They are working with the same baud rate and not working at the same time. Thanks KH2011-05-17 3:09 AM
Yes, if you set them to operate in mode 1, which is the standard asynchronous mode.
Han-Way HuangWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.