2016-01-12 6:18 AM
Hello,
I need help with regard to extending the 4 microphone architecture of X-CUBE-MEMSMIC to 6 microphones using X-NUCLEO-CCA02M1 and STEVAL-MKI155V3. I have attached the modified BSP driver .c and .h files. Also in audio_application.h I have changed the no. of microphones to 6. I have tried to configure SPI3 for microphones M5 and M6. I see that slave select for both SPI1 and SPI3 are the same and since the slave select is not being used in this case, I know this shouldnt be a problem. Can you please let me know which all part of the code should I look into to get it working for 6 microphones. I have also tried to increase the PDM buffer but have not been successful. I see that PDM data is available on scope on all the 4 microphones but due to changes from my part of the code the data is not being recorded. Apart from the x_nucleo_cca02m1_audio_f4 BSP driver which part I should look into to extend the same to 6 microphone architecture. Thanks, Ramya2016-08-21 10:34 PM
en.X-CUBE-MEMSMIC1
I want to add this to stm32cube but say this verison is not for this stm32cube release STM32CubeExpansion_MEMSMIC1_V1.3.0STM32Cube_FW_F4_V1.12.02016-08-21 10:54 PM
Hi
STM32CubeMX 4.16 dont support X-CUBE-MEMSMIC1 1.3.0, I want run sample code but when do with install path
STM32CubeMX
say:
STM32CubeMX version or tell me solution
''doesn't apply to this version of
STM32CubeMX ''
please note
STM32CubeMX 4.16 dont support X-CUBE-MEMSMIC1 1.3.0, I want run sample code but when do with install path
STM32CubeMX
say:
STM32CubeMX version or tell me solution
thx Ahrovan
2016-12-01 9:25 AM
Hi Ahrovan,
Sorry for late reply.For what concern the support on STM32 features i would suggest you to contact STM32 support teamRegards,AlessandroWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.