2014-05-26 12:10 AM
What are the basic features of VL6180X ?
#vl6180x #features2014-05-26 11:20 AM
The VL6180X allows any user to measure the distance of any object within a 0 to 100mm range from the sensor regardless of the reflectivity of the material. Along with the distance measured, the VL6180X gathers information on the amount signal and noise entering into the sensor which allows the VL6180X to measure the distances of these objects in any lighting environment.
The VL6180X also allows a user to measure the amount of ambient light with the built in ambient light sensor. With a simple math equation the equivalent lux value can be obtained from the measurement stored in the VL6180X.2015-02-06 11:33 AM
What is the sampling rate range for the ambient light sensor?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.