2015-03-07 2:49 PM
I have a one of the VL6180x sensors that I have soldered leads onto and configured as specified in the datasheet.
Using this library on GitHub I'm able to read ambient light measurements, but range measurements are not working:https://github.com/sparkfun/ToF_Range_Finder-VL6180_LibraryI'm reading a value of 255 for the range measurement and the (0x004D)RESULT_RANGE_STATUS registers bits[7:4] contains a value of 1 which is described in the app notes AN4545 as a system error.After looking over the code from GitHub I'm not too confident in it. I've spent a few hours making changes and applying some of the suggestions here in the forum that I believe are relevant. However, I want to make sure that it is a software issue before I go much further.What would cause a system error 1?Module info:Model ID = 180Model Rev = 1.3Module Rev = 1.2Manufacture Date = 15/9/14 Phase: 1Manufacture Time (s)= 19898-Jonathan2015-03-09 12:28 PM
2015-03-10 11:34 PM
From: Ken W@STPosted: Monday, March 09, 2015 8:28 PMSubject: VL6180x System error code after single shot range measurement attemptA ranging error of 1 is caused by a failure of VCEL continuity test. This is can be caused by: 1. AVDD_VCEL (pin 8) not connected well and powered by 2.8V. 2. AVSS_VCEL (pin 9) not connected to GND 3. An internal problem with the laser in which case the part should be replaced.Ken W@ST
2015-04-17 6:05 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.