2018-11-26 5:42 AM
I consider to use VL6180X sensor in a closed-loop system to measure a distance from the object.
1) I would like to sample distance measurement at 100-500 Hz. But if I read the manual correctly, even in continuous mode I can get measurements at best at ~100 Hz (assuming RangeSetMaxConvergenceTime is 4ms). Is it correct?
2) Do I understand correctly that the minimal distance measurement increment is 1mm?
Thanks, Andrei
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.