2020-04-24 2:05 AM
Hallo everybody,
I'm still very inexperienced with the board and the tools.
I start Unico and contact the STEVAL-MKI109V3 and get the following error:
Please can someone give me a hint on how I can update the STEVAL-MKI109V3 board and where I can get the latest firmware from?
I have already installed the STM32CubeProgrammer.
When trying to switch the STEVAL-MKI109V3 board into DFU mode, the board appears in the Windows 10 Device Manager as "STM32 BOOTLOADER".
Many thanks
Carsten
Solved! Go to Solution.
2020-04-24 4:03 AM
Hallo Eleon,
thank you for the quick answer. I solved the Problem. Since the STEVAL-MKI109V3 board went into the Bootloader-Mode instead of the DFU mode I wrote the *.bin-file which I found in the UNICO-DIR into the Device. And now it works.
So thanks a lot and have a nice weekend...
Best regards
Carsten
2020-04-24 3:35 AM
Hi @Carsten , I cannot see the error message in your post (you should upload the screenshot via the Image button you can find in the bottom bar). Btw, to set the STEVAL-MKI109V3 board in DFU mode you have to:
Then you can follow the instructions in the attached video on how to set the STM32 Programmer to download the .bin FW file on a board via DFU.
Please note that if you have the drivers of the DfuSe demo tool installed, they may conflict with the one of the STM32Programmer.
Regards
2020-04-24 4:03 AM
Hallo Eleon,
thank you for the quick answer. I solved the Problem. Since the STEVAL-MKI109V3 board went into the Bootloader-Mode instead of the DFU mode I wrote the *.bin-file which I found in the UNICO-DIR into the Device. And now it works.
So thanks a lot and have a nice weekend...
Best regards
Carsten
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.