2016-03-15 9:48 AM
The LIS3DH works from 1.8V to 3.6V.
If I use it direct from a CR2032 coin cell w/o regulator, will there be any side effects as the voltage drops from 3.3V to ~2.2V?For example, will the calibration drift substantially?Is this something that I can adjust for in FW?If other devices on the same VCC cause the VCC to drop 0.1V to 0.2V over ~ millisecond, can this cause false triggers on the LIS3DH?I am not using the ADC, only the accelerometer.Thanks #lis3dh #accelerometerWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.