2015-05-02 4:38 AM
Good morning guys. I'm writing because I need help for interfacing an Inemo M1 with a STM32F4. I have the need to take all the sensor values of Inemo on F4 via USART. I used to start the sample code of 'Inemo called ''AHRS_LIB_Continuos'' and I implemented a small library for port configuration USART1 that I post below:
#include ''inemo_usart_interface.h''#include ''iNemo_Led.h''/* PIN on J12 equal to Tx 6 (GPIOA9) e Rx 7 (GPIOA10)*/FlagStatus xUsartTxComplete;FlagStatus xUsartRxComplete;void usart1_IRQHandler(void);ErrorStatus usart_initialize() { USART_InitTypeDef usart_init; NVIC_InitTypeDef NVIC_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; /*Enable usart periph clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_USART1, ENABLE); /* Configure and enable usart1 interrupt */ NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_Init(&NVIC_InitStructure); /* Configure usart pins: RX and TX ---------------------------------*/ /* Configure MISO pin as Alternate Function Push Pull */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Init usart */ usart_init.USART_BaudRate = 512000; usart_init.USART_WordLength = USART_WordLength_8b ; usart_init.USART_StopBits = USART_StopBits_1; usart_init.USART_Parity = USART_Parity_No; usart_init.USART_Mode = USART_Mode_Rx; usart_init.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_Init(USART1, &usart_init); USART_Cmd(USART1, ENABLE); USART_ITConfig(USART1, USART_IT_TXE, ENABLE); USART_ITConfig(USART1, USART_IT_RXNE, ENABLE); xUsartRxComplete = USART_GetFlagStatus(USART1, USART_IT_RXNE); xUsartTxComplete = USART_GetFlagStatus(USART1, USART_IT_TXE); iNEMO_Led_Toggle(LED1); return SUCCESS;}void usart_raw_receive(uint8_t *data, uint16_t length) { uint16_t i; uint8_t rxbyte; for(i=0; i<length; i++) { rxbyte = USART_ReceiveData(USART1); data[i] = rxbyte; while(xUsartRxComplete != SET); xUsartRxComplete = RESET; } // if(data[0] == 0xAA){iNEMO_Led_Toggle(LED1);};}void USART1_IRQHandler(void) { if (USART_GetITStatus(USART1, USART_IT_TXE) != RESET) { xUsartTxComplete = SET; USART_ClearITPendingBit(USART1, USART_IT_TXE); } else if(USART_GetITStatus(USART1, USART_IT_RXNE) != RESET) { xUsartRxComplete = SET; USART_ClearITPendingBit(USART1, USART_IT_RXNE); }} Given that the transmission from the F4 working properly, because already tested, I need to run the rx and tx on 'Inemo. Do you believe that I have to change something in the example code (for example vector table or other things ) and in my library? In particular in this case I'm trying to send a byte from F4 to inemo to test the communication, but it doesn' t work.Thank you. I await answers.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.