2021-08-24 3:12 AM
I want to readout the STSS22H, without any polling or I2C clock stretching. I want to use the following sequence:
Is this possible with the STSS22H, where can I find the maximum conversion time in one **** mode? This information is missing in the datasheet.
Solved! Go to Solution.
2021-08-25 9:01 AM
Hi, the conversion time should depend from the ODR you set: the limit is 1Hz, so a complete conversion will take 1s. For higher ODRs, the conversion time will be lower (for example for ODR=25Hz the conversion time will be 1/25s = 40ms).
\DK
2021-08-24 5:17 AM
Does this help?
2021-08-24 11:44 PM
No, it's a bit vague, does it mean that the sampling takes around 1000ms, seems a bit long.
2021-08-25 9:01 AM
Hi, the conversion time should depend from the ODR you set: the limit is 1Hz, so a complete conversion will take 1s. For higher ODRs, the conversion time will be lower (for example for ODR=25Hz the conversion time will be 1/25s = 40ms).
\DK
2021-08-26 6:55 AM
Ok, then I will go with freerunning mode at a high ODR. Can I just sample the data registers without checking for the data ready flag (I just need a most recent sample, no sync of any kind needed), or will this cause I2C clock stretching?
I've got this running in a freeRTOS thread, but sometimes the BUSY bit of the I2C peripheral (STM32F4) gets stuck, i'm suspecting due to clock stretching.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.