cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-STWINBX1 examples doesn't respect STM32U585 datasheet

nicolas
Senior II

The datasheet of STM32U585 say that "For operation with voltage higher than Min (VDD, VDDA, VDDUSB, VDDIO2) +0.3 V, the internal pull-up and pull-down resistors must be disabled." (chap. 5.3.1).
The STEVAL-STWINBX1 use a VDDA of 2.75V and a VDD of 3.3V => Min (VDD, VDDA, VDDUSB, VDDIO2) +0.3 V = 3.05V < VDD = 3.3V.
But in the examples provided for STEVAL-STWINBX1, pull up and down are used with a VDD of 3.3V.
So which is correct, the datasheet or the examples ?

4 REPLIES 4
Amel NASRI
ST Employee

Hi @nicolas ,

Reviewing the product datasheet, I think that you are referring to the following note:

AmelNASRI_0-1760026503246.png

This note is applicable for VIN (the voltage input that may be applied for device pins) and not to VDD:

AmelNASRI_1-1760026546342.png

Therefore, I believe that the STEVAL-STWINBX1 design aligns well with the operating conditions described in the datasheet and in AN5373Getting started with STM32U5 MCU hardware development.

Additionally, I received confirmation that the STEVAL-STWINBX1 has been used for a considerable time with various firmware and demos without any reported issues.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I'm using SDDataLogFileX with STEVAL-STWINBX1. In the code i saw that pull up are used for I2C2 (I2C2_MspInit). When measuring on the I2C2 pins, i saw a signal that go up to ~3.2V. So for my understanding it doesn't respect the datasheet because it's higher than 2.75V + 0.3V.

I assume that there is no external voltage input for the I2C pin, so it is normal that the voltage is aligned with VDD.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I also found it normal but the datasheet say otherwise.

By reading the phrase "For operation with voltage higher than Min (VDD, VDDA, VDDUSB, VDDIO2) +0.3 V, the internal pull-up and pull-down resistors must be disabled.", for me the internal pull up should be connected to the minimum of those VDD so in the STEVAL-STWINBX1 case to the VDDA = 2.75V. 

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.