2024-10-18 8:48 AM
I tried all 3 available demos: default, FP-AI and Datalogger.
At last I flashed the original default demo back. All tests are done USB-powered or with LiPo.
Establishing a BLE connection with iPhone works in 10% of the cases.
Using an Android smartphone is more successfully.
All issues found:
- No plot data of gyro and accelerometer, but FFT and Board Pred Maintenance worked.
- In plot data the axes and 3 colored lines were shown at zero level, but no lines are changing (regardless autoscale setting).
- FFT shows sometimes lines horizontically like in plot data, no vertical bars and frozen.
- Or no sensor data at all, but I can turn on/off LED (very nice)
- Or plot data does not scroll, lines were drawn back and forth
- BLE interrupted on iPhone
Version FW: WB5MMG_STSW-PROTEUS_1.1.0 (from STEVAL-Proteus1 package) BLE-CbM
Having the latest BLE stack from Github (V1.20.0 build 2), because one ST employee noticed an older one (V1.19.0) in the current STEVAL-Proteus1 package.
I tried to show the demo to a customer in their factory and it ended not well.
Do I have to wait for STEVAL-Proteus 1.2.0 ?
Best regards
Solved! Go to Solution.
2024-11-13 6:22 AM
Hi @Joerg Wagner ,
The new STSW-PROTEUS v1.1.1 release is available on st.com
I suggest you update the BLE stack to version 1.19.0 to enable the low-power functionality used by STSW-PROTEUS.
Note that after installing STSW-PROTEUS v1.1.1 via FUOTA, you need to power off the board.
2024-11-13 6:22 AM
Hi @Joerg Wagner ,
The new STSW-PROTEUS v1.1.1 release is available on st.com
I suggest you update the BLE stack to version 1.19.0 to enable the low-power functionality used by STSW-PROTEUS.
Note that after installing STSW-PROTEUS v1.1.1 via FUOTA, you need to power off the board.
2024-11-14 8:54 AM
Hi Federica,
Thank you for the information.
Looks good!
All issues I mentioned are fixed with STSW-PROTEUS1 v1.1.1.
I suggest to use the BLE stack version 1.20.0 from Github project STM32CubeWB, released 5 months ago.
Version 1.19.0 would be a downgrade, not an upgrade.
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.