2021-02-02 2:29 AM
Hi, st
Now I've found some new problems.
Sometimes the value read from who AMI register will be 0x48. After finding this problem, I suspect that the connecting wire is unstable. After replacing the DuPont wire, the value read back to normal (0x6b). I want to ask what is the reason for this strange phenomenon.
In addition, I found that the accelerometer data rate can only be set at 833hz or below. If the accelerometer data rate is set above 1667hz (1667hz,3333hz,6667hz), the value read from the register is still the previous value, that is, the data setting above 1667hz always fails. By the way, there is no such phenomenon in the setting of gyroscope.
So I updated the driver file to the version of 5 days ago (ism330dhcx: fixed examples # 107) in Git library.
A step was added to the driver calling routine of this version(ism330dhcx_device_conf_set), but this step didn't seem to succeed.
After execution, I also read the value of this register(ism330dhcx_device_conf_get(&dev_ctx, &rst)), and the returned value is 0(rst == 0).
In other words, the device_conf bit is not really set to 1 and remains in the default state after the set is executed.
But according to the datasheet, it seems that this bit must be set to 1 to write the new configuration normally?
Now I'm a little confused, can you help me answer the three questions of appeal?
Best regards
June6
2021-02-02 6:05 AM
Hi @6June.1 ,
about the "instability" of the WHO_AM_I value, are you communicating with SPI or with I2C protocol? Especially in this second case, I'm afraid that there vas some connection unstable that prevented the WHO_AM_I content to be properly transmitted, losing some bits but anyway transmitting the ACK signal, making the MCU able to decode a value that however was not the proper register content. But I would suggest you to use an oscilloscope to check the integrity of the transmitted data.
About the ODR 833Hz setting limit for the accelerometer, are you referring the maximum accelerometer bandwidth configurations, i.e. the maximum signal you can detect? This is determined by the ODR and in effect as you can see from the Table 61 of the datasheet the bandwidth is defined up to 833Hz. For the gyroscope, however, the full band is available, especially for imaging stabilization applications, that require high gyroscope resolution and a broad band. This is due to mechanical characteristics of the two sensors.
Coming to your last question:
>>But according to the datasheet, it seems that this bit must be set to 1 to write the new configuration normally?
Is the DEVICE_CONF the only bit that you are not able to set with the Github procedure? I mean, you set it and when you read back the register content, that bit is returned to 0, right? This should have anyway been set, and the configuration procedure can go on. Are you facing issues in reading the device outputs?
Please let me know if these considerations ca answer your questions.
-Eleon
2021-02-02 6:34 AM
2021-02-02 7:57 PM
By the way, we only need to collect acceleration data, but the demand for sampling rate is relatively high. What's your suggestion.
That's why I ask you, the accelerometer ODR can't be set to 6667 Hz.
2021-02-02 8:18 PM
The current configuration status is as follows
/* Start device configuration. */
ism330dhcx_device_conf_set(&dev_ctx, PROPERTY_ENABLE);
ism330dhcx_device_conf_get(&dev_ctx, &rst);
// if (rst != PROPERTY_ENABLE)
// TODO Define return value
// return 4;
/* Enable Block Data Update */
ism330dhcx_block_data_update_set(&dev_ctx, PROPERTY_ENABLE);
ism330dhcx_block_data_update_get(&dev_ctx, &rst);
if (rst != PROPERTY_ENABLE)
// TODO Define return value
return 5;
/* Set Power Mode */
ism330dhcx_xl_power_mode_set(&dev_ctx, ISM330DHCX_HIGH_PERFORMANCE_MD);
ism330dhcx_xl_power_mode_get(&dev_ctx, &rst);
if (rst != ISM330DHCX_HIGH_PERFORMANCE_MD)
// TODO Define return value
return 6;
/* Set Output Data Rate */
ism330dhcx_xl_data_rate_set(&dev_ctx, ISM330DHCX_XL_ODR_6667Hz);
ism330dhcx_xl_data_rate_get(&dev_ctx, &rst);
if (rst != ISM330DHCX_XL_ODR_6667Hz)
// TODO Define return value
return 7;
/* Set full scale */
ism330dhcx_xl_full_scale_set(&dev_ctx, ISM330DHCX_16g);
ism330dhcx_xl_full_scale_get(&dev_ctx, &rst);
if (rst != ISM330DHCX_16g)
// TODO Define return value
return 8;
memset(&pin_int1_route, 0, sizeof(pin_int1_route));
pin_int1_route.int1_ctrl.int1_drdy_xl = PROPERTY_ENABLE;
ism330dhcx_pin_int1_route_set(&dev_ctx, &pin_int1_route);
ism330dhcx_pin_int1_route_get(&dev_ctx, &pin_int1_route);
if (pin_int1_route.int1_ctrl.int1_drdy_xl != PROPERTY_ENABLE)
// TODO Define return value
return 9;
ism330dhcx_pin_mode_set(&dev_ctx, ISM330DHCX_PUSH_PULL);
ism330dhcx_pin_mode_get(&dev_ctx, &rst);
if (rst != ISM330DHCX_PUSH_PULL)
// TODO Define return value
return 10;
ism330dhcx_pin_polarity_set(&dev_ctx, ISM330DHCX_ACTIVE_LOW);
ism330dhcx_pin_polarity_get(&dev_ctx, &rst);
if (rst != ISM330DHCX_ACTIVE_LOW)
// TODO Define return value
return 11;
ism330dhcx_all_on_int1_set(&dev_ctx, PROPERTY_ENABLE);
ism330dhcx_all_on_int1_get(&dev_ctx, &rst);
if (rst != PROPERTY_ENABLE)
// TODO Define return value
return 12;Following the above steps, there are two problems.
2021-02-03 7:50 PM
I have understood what is written in the datasheet. Under mode 1, the maximum sampling rate of the accelerometer can only reach 833hz. In order to reach 6667hz, mode 4 must be used.
Do you have any routines related to mode 4 using interrupt? Or briefly explain the following process to me, only part of which is described in application note.
2021-02-05 4:37 AM
Hi @6June.1 ,
Mode 4 refers to the auxiliary SPI interface used in OIS applications, so you have to wire these additional lines to your application processor to use it, but ok, in this way you could deploy the 6.66kHz ODR speed.
Since there is yet no application note available for the ism330dhcx, i suggest you to use the lsm6dso one (AN5192), where Mode 4 is detailed. This digital feature is shared between these two sensors. In page 85 you can find the pseudocode for Mode 4 routine configuration:
1. Wait 10 ms // Boot time
// Device in power-down after this time period
2. Write 31h to CTRL1_OIS // Turn gyro on through Auxiliary SPI 3-write interface
// (OIS Gyro: FS = ±250 dps / ODR = 6.66 kHz)
// Enable Mode 4 (Mode4_EN = 1)
3. Write 00h to CTRL3_OIS // Set XL through Auxiliary SPI 3-wire interface
// (OIS XL: FS = ±2 g / ODR = 6.66 kHz)
4. Wait 74 ms // Gyroscope max turn-on time is 70 ms
// Selected LPF1 (00b) settling time is 4.05 ms
// (27 samples @ 6.66 kHz)
// Selected LPF OIS (000b) settling time is 2.85 ms
// (19 samples @ 6.66 kHz)
5. Read output registers 22h to 27h // Read gyroscope output data through Auxiliary SPI
6. Read output registers 28h to 2Dh // Read accelerometer output data through Auxiliary SPILet me please know if these indications can help you.
-Eleon
2021-02-06 5:33 AM
The current situation is that if the parameters are written into CTRL1_OIS and CTRL3_OIS registers by the auxiliary SPI bus, the parameters read by the auxiliary SPI are still the default values, and the parameters read by the primary SPI bus are the parameters I write.
Moreover, when the auxiliary SPI is used to read the value of 1eh register, the new data is never available. And the auxiliary SPI is used to read the values of 22h to 27h registers and 28h to 2dh registers, and the data is always 00h.
If you use the primary SPI bus to read and write, everything is normal.
I can't figure out what causes this phenomenon...
I hope you can point out the problem.
-June6
2021-02-24 9:42 AM
Hi @6June.1 ,
sorry for my late answer... Which mode are you running before activating the OIS chain (Mode3/Mode4)?
From the LSM6DSO app note, p.76: if the accelerometer is configured in Ultra-Low-Power mode when enabling the OIS (Mode 3 or Mode 4) is required, the device must be configured in Power-Down mode before enabling the OIS chain.
-Eleon
2025-01-14 3:55 AM
Hi,
I am using ISM330 sensor with 'Arduino nano connect' and STM32duino ISM330HDCX libraries. It seems working well with the ODR up to 416 (Hz) but the ODR higher than that could not be achieved. I read the register CTRL1_XL (10h) register after setting the ODR, it shows the value it supposed to be. The sensor is in high performance node and reading register CTRL6_C (15h) confirms it. Is there any further settings I need to do to achieve higher ODR?
BTW I am using I2C bus for reading the FIFO data once the number of samples go above a threshold value.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.