2025-03-18 6:08 AM - last edited on 2025-03-26 3:53 AM by Amel NASRI
Hello, community!
I recently purchased the SensorTile Box Pro to conduct various educational experiments. It connects via Bluetooth to my phone, but when I try to connect it to my laptop using the MEMS STUDIO application, it does not work via either USB or Bluetooth. I receive a red error message stating that the board is not identified.
I have tried on three different PCs, both on Windows 10 and Windows 11, but it still does not work. All the necessary drivers have been installed, and I have no explanation for why it is not being recognized. I should mention that my laptop is running Windows 10.
Can you help me?
Solved! Go to Solution.
2025-04-10 7:20 AM
Hi @Ats6 ,
In order to connect the STEVAL MKBOXPro to MEMS Studio, you have to either upload the dedicated FW in the Firmware folder of MEMS Studio (USB c serial communication) or create the FW with Algobuilder to communicate via Bluetooth. It cannot use the FW compatible with the mobile app.
2025-04-10 7:20 AM
Hi @Ats6 ,
In order to connect the STEVAL MKBOXPro to MEMS Studio, you have to either upload the dedicated FW in the Firmware folder of MEMS Studio (USB c serial communication) or create the FW with Algobuilder to communicate via Bluetooth. It cannot use the FW compatible with the mobile app.
2025-04-10 9:33 AM
Hi @Federica Bossi! Is there any tutorial or topic on this topic? I'm a beginner with the platforms and devices from stmicroelectronics and something more concrete and easy to understand could help me. Thank you!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.