2024-10-08 2:06 PM - edited 2024-10-08 3:06 PM
Hi
I have a custom pcb design with a lsm6dsv and lsm303agr. So far it is only streaming xyz coordinates.
I need to come up with something like a rotating dice in this Video at minute 5:20 :https://www.youtube.com/watch?v=1mV_L-KEMy0
In fact i need to Show the orientation of human head and not a dice.
Which Tutorial or example project do you recommend as starting point?
Is it correct that with lsm6dsv the Gyro has a good Performance, so i dont even need the magnetometer for drift correction?
Is lsm6dsv the right chip, or is a better pin compatible chip in the lsm6 family?
Solved! Go to Solution.
2024-11-08 7:25 AM
Hi @MK..1 ,
You can look at this article.
In addition, the user manual of the MotionFX could be helpful!
2024-11-08 7:25 AM
Hi @MK..1 ,
You can look at this article.
In addition, the user manual of the MotionFX could be helpful!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.