cancel
Showing results for 
Search instead for 
Did you mean: 

Question for LPS25HB Pin#7 connection

genki
Associate

I am designing to mount LPS25HB on the board.

Communication is I2C.

Please help me with the connection of Pin 7 (INT_DRDY).
Is this pin an open pad? Or does it need to be connected to GND?

1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @genki ,

Welcome to ST Community!

INT_DRDY pin is an output of the device. If not used can be left floating. In other case it must be connected to GPIO of microcontroller to verify the features of this pin (see page 37 of LPS25HB datasheet)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Federica Bossi
ST Employee

Hi @genki ,

Welcome to ST Community!

INT_DRDY pin is an output of the device. If not used can be left floating. In other case it must be connected to GPIO of microcontroller to verify the features of this pin (see page 37 of LPS25HB datasheet)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.