2020-06-23 2:26 PM
I have recently got a brand new Sensortile and a nucleo L476RG.
I checked if the tile was working by connecting the tile to the cradle expansion board (STLCX01V1) and using the bluetooth app from ST (STBLESensor). The system worked and I could view data being streamed to the app.
In order to view the data to the PC, I decided to solder the tile to the mini cradle (the one with SD card and battery slot, STLCR01V1), connected the SWD interface the Nucleo, removed the CN2 jumper and connected the Nucleo to the computer via the USB cable. I observed three things.
When I instead connect the cradle to the USB port of the computer, a solid red LED is seen on the cradle, but no hardware is detected.
Surprisingly, when I connect the battery to the mini cradle, the cradle LED turns green, and the orange LED on the tile starts flashing again and I can read the data from the STBLESensor app, this proves that the tile is working fine.
Any suggestions on what am I missing on the steps required to program the sensortile via the Nucleo?
Solved! Go to Solution.
2020-06-23 2:56 PM
Ok I found out you need to connect the battery to the mini cradle for the system to work. Pretty weird as I thought the USB connection to the mini cradle would be enough.
2020-06-23 2:56 PM
Ok I found out you need to connect the battery to the mini cradle for the system to work. Pretty weird as I thought the USB connection to the mini cradle would be enough.
2021-10-21 2:41 AM
i am facing the same problem even after connecting the battery,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.