cancel
Showing results for 
Search instead for 
Did you mean: 

Obsolescence of IIS328DQTR and equivalent components

Hey! 

If I well understood the component IIS328DQTR will be at least "NRND" in 2025. 

The IIS3DHHC seems to be a good substitute but it doesn't have all the interrupt features of the IIS328DQTR. 

Can you confirm the lifetime of the IIS328DQTR? 

Do you have a 3-axis digital accelerometer with the feature: "The device may be configured to generate an interrupt signal through inertial wakeup events, or by the position of the device itself."

Kind regards

Charles D

 

1 REPLY 1
Federica Bossi
ST Employee

Hi @CharlesD_4_ElsysDesign ,

from 2025 the commitment ends and thereafter its availability will depend on market conditions. However, we recommend for new designs to consider newer generation products such as IIS2DLPC

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.