2019-09-03 8:55 PM
I am IIS2DLPC accelerometer for Tilt Angle Measurement.
I have done 6 Axis Calibration. I can able to measure the Tilt Angle less the 1 degree accuary.
Is there any other way, I can measure less than 1 degree accuracy with out Calibration ??
Note : Creating Perfect Calibration Setup to Expose 1g gravity on the Accelerometer axis is a overhead for us.
Please Suggest any ST Accelermeter which can give 1 min accuracy with out calibration.
2019-09-04 8:22 AM
Hi @SM.19 , being your target application the inclinometer, I suggest you to use the IIS3DHHC device, which is of course more accurate. It should be able to reach the required 1deg accuracy, especially in a controlled environment (limited temperature swing and limited ambient noise). Is this device matching your requirements? Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.