2020-08-02 5:42 PM
I had a device that need to record data then plot the location. What type of mems sensor should I use?
Will it give the location or just reference.
CS
2020-08-07 2:34 AM
Hi @ChawCS ,
the state of the art for plotting the location of a device make use of GPS modules because MEMS motion sensors are not able to provide data that can be analysed to plot a position in a 2/3D environment with enough accuracy.
Anyway, if you would like to research how accurate the plot from MEMS sensors data can be, you can try any accelerometer, like LIS2DW12, or even a 6-axis module, that can help with gyroscope data, like LSM6DSOX.
does this help you?
Niccolò
2020-08-07 5:27 PM
Hi Niccolo,
As this device (mobile car) will be in-house, do you think GPS can do the job?
Think a reference distance will do, mean the device move left, right. As it is to guide a curve line, as in a circle.
Regards
ChawCS
2020-08-10 6:43 AM
Hi @ChawCS,
I did not kept into consideration the distances you have to work with. for a precise positioning of this kind I don't think GPS is suitable.
So I would try to use a LSM6DSOX (6-axis module) to try to solve this problem. Maybe you will not have a perfect positioning, but, with the right references around the device, it can be done.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.